Our energy working fo you.

Patches

 Locate patch and click on its executable link to download.

 

Product                     

Version  

Description                                                        

Patch                               

InPower Pro NA  

1. This patch is specifically designed for InPower PRO versions V15.0.4.25130 and V16.0.

2. It is compatible with Windows 10 and Windows 11 operating systems.

3. Before installing the patch, ensure that all InPower tools and related utilities are closed.

4. The patch will be automatically uninstalled if the main application (V15.0 or V16.0) is removed.

Fixed issues

This patch specifically resolves issues related to XY table feature (FDL) writing issue and PCC3100 Connection Issue in the InPower Pro application versions V15.0.4 and V16.0.

InPower_Interim_Patch

InPower Onan                    

NA  

 

1. This patch is specifically designed for InPower Onan versions V15.0.4.25130 and V16.0.

2. It is compatible with Windows 10 and Windows 11 operating systems.

3. Before installing the patch, ensure that all InPower tools and related utilities are closed.

4. The patch will be automatically uninstalled if the main application (V15.0 or V16.0) is removed.

Fixed issues

This patch specifically resolves issues related to PCC1302 calibration and feature writing in the InPower Onan application versions V15.0.4 and V16.0.

 

 InPower ONAN_PCC1302_Patch

InPower Pro
InPower Lite
InPower Onan
V15.0.4

1.  This patch shall work for ETools V14.5 and V15.0 only.

2.  Patch V15.0.4 supports Windows 10 and Windows  11 operating systems only.

3.  Patch V15.0.4 cannot be installed without administrative privileges.         

4.  All InPower tools and their utilities should be closed before installing the patch.

5.  The Patch is uninstalled automatically when the Main application (V14.5 or V15.0) is uninstalled.

6.  If multiple tools are to be installed on a particular machine, then it is recommended to install the patch after ALL the tools are installed. Patch will have NO effect if another tool is installed post patch installation.

New features & Enhancements

 1.      Security improvements.

 2.      InCal server migration for InCal Extractor.

Important Notice: Users must upgrade to version 15.0.4 to continue accessing new PGA files.

InPower Patch V15.0.4.25130
InPower Pro
InPower Lite
InPower Onan
V15.0.3

1.  This patch shall work for ETools V15.0 only.

2.  Patch V15.0.3 supports Windows 10 and Windows 11 operating systems only.

3.  Patch V15.0.3 cannot be installed without administrative privileges.         

4.  All InPower tools and their utilities should be closed before installing the patch.

5.  The Patch is uninstalled automatically when the Main application V15.0 is uninstalled.

6.  If multiple tools are to be installed on a particular machine, then it is recommended to install the patch after ALL the tools are installed. Patch will have NO effect if another tool is installed post patch installation.

New features & Enhancements

1.  For the Raven EFI - CARB 2024 Emission Requirement, the InPower application will identify the existing calibration part number in the Raven controller (Device ID 72). Initial calibration will be restricted if an old calibration part number (A030G041) is selected when a controller is already calibrated using new part number(A074V714) but can proceed on the old calibration if the new part number is used. 

InPower Patch V15.0.3.25503
InPower Pro
InPower Lite
InPower Onan
V15.0.2

Fixed issues

1.This patch shall work for ETools V15.0 and Patch V15.0.2.24313.


2. This patch is used to fix PCID fluctuation issue only.


3. This Patch will update files related to PCID Change.


4. After installing the Patch, manual registration is required.


5. This patch is strictly used only for PCID ISSUE

InPower_PCID_Issue_Fix
InPower Pro
InPower Lite
InPower Onan
V15.0.2

1.  This patch shall work for ETools V15.0 only.

2.  Patch V15.0.2 supports Windows 10 and Windows 11 operating systems only.

3.  Patch V15.0.2 cannot be installed without administrative privileges.         

4.  All InPower tools and their utilities should be closed before installing the patch.

5.  The Patch is uninstalled automatically when the Main application V15.0 is uninstalled.

6.  If multiple tools are to be installed on a particular machine, then it is recommended to install the patch after ALL the tools are installed. Patch will have NO effect if another tool is installed post patch installation.

New features & Enhancements

1.  Auto Registration will work for users with new WWID formation.

2.  Engineering tool - IDA logger will work for more than 10k byte IDA Log table.

3.  For CCS controller, product strings changed to "CONTROLLER-CYL CUTOFF SYSTEM and FEATURE-CYL CUTOFF SYSTEM"

Fixed issues

1. PCID fluctuation issue has been resolved.

InPower Patch V15.0.2.24313
InPower Pro
InPower Lite
InPower Onan
V15.0.1

1. This patch shall work for ETools V15.0 only.

2.  Patch V15.0.1.24109 supports Windows 10 and Windows 11 operating systems only.

3.  Patch V15.0.1.24109 cannot be installed without administrative privileges.             

4.  All InPower tools and their utilities should be closed before installing the patch.

5.  The Patch is uninstalled automatically when the Main application V15.0 is uninstalled.

6.  If multiple tools are to be installed on a particular machine, then it is recommended to install the patch after ALL the tools are installed. Patch will have NO effect if another tool is installed post patch installation.

New features & Enhancements 

1. Added Rover device (ID_149) support. 

2. Included Cummins Inc. Update Manager to install new updates.

Please contact your distributor or Cummins contact personnel for any queries related to the patch. 

For any assistance and help regarding installation and uninstallation of the patch, feel free to write to "InPower.Support@cummins.com"

InPower Patch V15.0.1.24109
InPower Pro
InPower Lite
InPower Onan
V14.5.1

1. This patch shall work for ETools V14.5 only.

2.  Patch V14.5.1.23222 supports Windows 10 and Windows 11 operating systems only.

3.  Patch V14.5.1.23222 cannot be installed without administrative privileges.             

4.  All InPower tools and their utilities should be closed before installing the patch.

5.  The Patch is uninstalled automatically when the Main application V14.5 is uninstalled.

6.  If multiple tools are to be installed on a particular machine, then it is recommended to install the patch after ALL the tools are installed. Patch will have NO effect if another tool is installed post patch installation.

New features & Enhancements 

1.  TPL file format changed to Guidanz Compatible JASON format.

2.  Connection Error Screen will display additional informative messages.

3.  QSOL documentation update for Win 8 obsolescence

4.  Firmware version manager is now capable of handling multiple calibrations for single device ID.

Fixed issues

For PCC3300V1 strategic build #A066N050, tool will display correct informative message related to the latest version of calibration file.

InPower_Patch_V14_5_1_23222